About changing the voltage for NVCC_CSI & NVCC_EIM in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About changing the voltage for NVCC_CSI & NVCC_EIM in i.MX6DQ.

Jump to solution
910 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. 

My customer is considering that changing the VGEN4's voltage from 1.8V to 3.3V via I2C in operation.

But, the VGEN4 output to NVCC_CSI & NVCC_EIM in i.MX6DQ.

Is it possible to accept the changing the voltage for NVCC_CSI & NVCC_EIM of i.MX6DQ in operation?

Best Regards,

Keita

Labels (2)
0 Kudos
1 Solution
627 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Yes, it is possible to change the voltage for NVCC_CSI & NVCC_EIM of i.MX6DQ in operation,

assuming all voltages are within the specified range, and external parts, connected to  the i.MX6 pins,

powered via  NVCC_CSI & NVCC_EIM, are tolerant to the applied voltages.

 

MMPF0100 I2C programming (alternatives) 

https://community.nxp.com/thread/343843 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
628 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Yes, it is possible to change the voltage for NVCC_CSI & NVCC_EIM of i.MX6DQ in operation,

assuming all voltages are within the specified range, and external parts, connected to  the i.MX6 pins,

powered via  NVCC_CSI & NVCC_EIM, are tolerant to the applied voltages.

 

MMPF0100 I2C programming (alternatives) 

https://community.nxp.com/thread/343843 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos