About capacitor value for some power supply in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About capacitor value for some power supply in i.MX6

Jump to solution
608 Views
tomo
Contributor II

Hello, all.

SABRE-SD board has 22uF capacitor for VDD_HIGH_CAP, NVCC_PLL_OUT pin.

But these pin are recommended a 10uF capacitor according to Design Checklist (IMX6DQ6SDLHDG_Rev1.pdf).

And it is written in checklist that operation cannot be guaranteed, if capacitance over 10uF.

Why SABRE-SD board has 22uF, and does SABRE-SD board not occurred problem so far?

Best regards,

Tomo

Labels (1)
0 Kudos
1 Solution
467 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tomo

to guarantee operation in whole temperature range

and production process variations it is necessary to

follow recommendations Design Checklist IMX6DQ6SDLHDG_Rev1.pdf.

Also SABRE-SD board design was developed before all processor

documentation was prepared.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
467 Views
tomo
Contributor II

My customer pointed out to me that 24 MHz crystal has stop once before stable oscillation.
Is this waveform good for the i.MX6?24M_XTAL.png

I changed to 22uF capacitor for NVCC_PLL_OUT pin, then 24 MHz oscillation stop phenomenon is not occured.
Could you tell me if this phenomenon is related to the value of the capacitor?

0 Kudos
468 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tomo

to guarantee operation in whole temperature range

and production process variations it is necessary to

follow recommendations Design Checklist IMX6DQ6SDLHDG_Rev1.pdf.

Also SABRE-SD board design was developed before all processor

documentation was prepared.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos