About burst transfer of SDMA in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About burst transfer of SDMA in i.MX6DQ.

Jump to solution
1,120 Views
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about burst transfer of SDMA in i.MX6DQ.

Refer to 22.5.8 AXI (Master) Bus Cycles Support in i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 1, 04/2013.

There are below descriptions.

=====

Only 32-bit word size accesses are supported for burst

mode accesses.

Only 8-bit (1 byte), 16-bit (2 byte) and 32-bit (4 byte) word

size supported for single access.

Maximum number of burst length is 16.

=====

=About DMA burst transfer=

When the burst accesses with following use case, is it supported except 32 bits word size access, too?

[Case.1]

Source : LPDDR2

Destination : EIM

[Case.2]

Source : EIM

Destination : LPDDR2

Keita

Labels (3)
0 Kudos
Reply
1 Solution
868 Views
Yuri
NXP Employee
NXP Employee

> When the burst accesses with following use case, is it supported except 32 bits word size access, too?

No. Only 32-bit aligned accesses should be used for WEIM bursts. 

View solution in original post

0 Kudos
Reply
2 Replies
869 Views
Yuri
NXP Employee
NXP Employee

> When the burst accesses with following use case, is it supported except 32 bits word size access, too?

No. Only 32-bit aligned accesses should be used for WEIM bursts. 

0 Kudos
Reply
868 Views
keitanagashima
Senior Contributor I

Do anyone have some update?

Keita

0 Kudos
Reply