About bit swapping of data lanes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About bit swapping of data lanes

跳至解决方案
2,145 次查看
okamotosatoshi
Contributor IV

Hi There,

I am designing LPDDR4 using i.MX8M Mini.

 

i.MX6 has the following restrictions on the data lane.

 ・D0, D8, D16, D24, D32, D40, D48, and D56 are fixed
 ・Other data lines free to swap within byte lane
  (Refer to the Hardware Development Guide)

 

i.MX8M Mini has the following description.

 ・Byte swapping within each 16-bit channel is OK. Bit swapping within each slice/byte lane is OK.
  (Refer to the Hardware Developer's Guide)

 

Is it okay to think that i.MX8M Mini has no restrictions to fix the lower bits ?

 

Best regards
- satoshi

0 项奖励
回复
1 解答
2,138 次查看
Yuri
NXP Employee
NXP Employee

@okamotosatoshi 

Hello,

   Yes, i.MX8M Mini has no restrictions to fix the lower bits.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,134 次查看
okamotosatoshi
Contributor IV

Hi Yuri

 

Thank you for your answer!

I understand that there are no restrictions to fix the lower bits.

I consider pin swaps according to the guidelines.

 

Best regards
- satoshi

0 项奖励
回复
2,139 次查看
Yuri
NXP Employee
NXP Employee

@okamotosatoshi 

Hello,

   Yes, i.MX8M Mini has no restrictions to fix the lower bits.

Regards,
Yuri.

0 项奖励
回复