About adjustment function of SDHC in i.MX6SDL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About adjustment function of SDHC in i.MX6SDL.

1,201件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about adjustment function of SDHC in i.MX6SDL.

I got the information that i.MX6 has Variable_Output_Data_Window(CMD19) function from below URL.

https://community.freescale.com/thread/334945

[Question]

[Q1]

When the adjustment specification of the SD card is tOP = 0~2[UI], is it possible to adjust regardless of the relation with the propagation-delay-time of the clock and data?

[Q2]

How is a sample point of host side fixed (adjusted) in Variable-clock function?

There is below description in SD Phsical Layer Specification V4.20.

"At the initialization step the host should take care to find the optimal sampling point for the card outputs."

Is this adjusted for the setup and hold to become a center?

(If it's yes, how much does the looseness occur?)

Best Regards,

Keita

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,087件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

please elevate this through local FAE

(reason is that I have big difficulties to understand questions).

Thanks.

Best regards

igor

0 件の賞賛
返信

1,087件の閲覧回数
keitanagashima
Senior Contributor I

Dear Igor,

Hello.

Sorry for my poor question.

I will re-post this question to understand easily.

So, I'll remove this request.

BR,

Keita

0 件の賞賛
返信