About aclk_sel field in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About aclk_sel field in i.MX6DQ.

Jump to solution
1,036 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I found the difference of aclk_sel field between Reference manual and source code.

First, Refer to aCCM_CSCMR1 register in IMX6DQRM(Rev.3).

CCM_CSCMR1[aclk_sel]

00 derive clock from PLL2 PFD2

01 derive clock from pll3_sw_clk

10 derive clock from AXI

11 derive clock from PLL2 PFD0

Next, "_clk_emi_set_parent" function in arch\arm\mach-mx6\clock.c of jb4.2.2_1.1.0.

00 derive clock from AXI

01 derive clock from pll3_sw_clk

10 derive clock from PLL2 PFD2

11 derive clock from PLL2 PFD0

Which is right description?

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
962 Views
igorpadykov
NXP Employee
NXP Employee

HI Keita

right is RM, also these settings are used in latest 3.14.28 BSP clk-imx6q.c

(emi_sels)

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
963 Views
igorpadykov
NXP Employee
NXP Employee

HI Keita

right is RM, also these settings are used in latest 3.14.28 BSP clk-imx6q.c

(emi_sels)

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply