About a pullup resistance value of JTAG_RESET_B of i.MX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About a pullup resistance value of JTAG_RESET_B of i.MX25

Jump to solution
564 Views
yuuki
Senior Contributor II

Dear all,

We release a product using i.MX25.
It is necessary for us to change the resistance parameter of the JTAG interface.

We pullup the RESET_B signal with 10K ohm according to the Schematic:SPF-23252.

MX25_JTAG.png

We want to change this register value to less than 1K ohm.

Would you tell me the minimum value of this register?
(Would you tell me about the other registers value?)

May I have advice?

Best Regards,
Yuuki

Labels (1)
Tags (2)
0 Kudos
1 Solution
484 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

JTAG_RESET_B is connected to cpu board SPF-26325 RESET_B (pin T18) ,

this resistance can be decreased and its value is limited

by jtag debugger port capability (please check its datasheet), not by i.MX25.

Best regards

igor
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
485 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

JTAG_RESET_B is connected to cpu board SPF-26325 RESET_B (pin T18) ,

this resistance can be decreased and its value is limited

by jtag debugger port capability (please check its datasheet), not by i.MX25.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos