Dear all,
We want to use external LCK and VSYNC.
In this case, we think that the IPU of i.MX6 makes a VSYNC of the output by using EXT_CLK and EXT_VSYNC.
And we understand that the actual output VSYNC delays from EXT_VSYNC.
Would you tell me the delay of actual VSINC for EXT_VSYNC?
(For example, 10 pixels or 20 pixels etc.)
Best Regards,
Yuuki
Hi Yuuki
EXT_VSYNC,EXT_CLK are not routed externally for i.MX6.
EXT_CLK is connected internally as shows
Table 18-3 : ipp_di_ _ext_clk connected to ipu_di_clk_root.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------