About a Wi-Fi module supported in AndroidL5.0 for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About a Wi-Fi module supported in AndroidL5.0 for i.MX6

ソリューションへジャンプ
3,934件の閲覧回数
yuuki
Senior Contributor II

Dear all,

AndroidKK4.4.x of i.MX6 supported a module of Atheros and Silex.

However, these are not listed in release note of AndoridL5.x.

Does AndoridL5.0 support a module of Atheros and Silex?

Best Regards,

Yuuki

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
3,785件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

L5.0.0 supports Silex, L5.1.1 not, refer to attached Release Notes

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,786件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

L5.0.0 supports Silex, L5.1.1 not, refer to attached Release Notes

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,785件の閲覧回数
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

Noted with thanks.

By the way, do you understand the reason not to support it in L5 .1.1?

Best Regards,

Yuuki

0 件の賞賛
返信
3,785件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

seems drivers are not available for L5.1.1,

since it uses more new kernel.

Best regards

igor

3,785件の閲覧回数
yuuki
Senior Contributor II

Dear Igor-san,

Thank you.

I understand.

Best Regards,

Yuuki

0 件の賞賛
返信