About a Wi-Fi module supported in AndroidL5.0 for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About a Wi-Fi module supported in AndroidL5.0 for i.MX6

Jump to solution
4,153 Views
yuuki
Senior Contributor II

Dear all,

AndroidKK4.4.x of i.MX6 supported a module of Atheros and Silex.

However, these are not listed in release note of AndoridL5.x.

Does AndoridL5.0 support a module of Atheros and Silex?

Best Regards,

Yuuki

Labels (2)
0 Kudos
Reply
1 Solution
4,004 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

L5.0.0 supports Silex, L5.1.1 not, refer to attached Release Notes

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
4,005 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

L5.0.0 supports Silex, L5.1.1 not, refer to attached Release Notes

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,004 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you for your support.

Noted with thanks.

By the way, do you understand the reason not to support it in L5 .1.1?

Best Regards,

Yuuki

0 Kudos
Reply
4,004 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

seems drivers are not available for L5.1.1,

since it uses more new kernel.

Best regards

igor

4,004 Views
yuuki
Senior Contributor II

Dear Igor-san,

Thank you.

I understand.

Best Regards,

Yuuki

0 Kudos
Reply