About VTT mode of SW4 on MMPF0100F1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About VTT mode of SW4 on MMPF0100F1

Jump to solution
703 Views
yuuki
Senior Contributor II

Dear all,

The SW4 of MMPF0100 has VTT mode.

When using F1 part number, SW4 is already programmed.

In MMPF0100F1, if SW4 is used as VTT mode, is SW4 of MMPF0100F1 re-programmable as VTT mode?

Best Regards,
Yuuki

Labels (1)
Tags (4)
0 Kudos
1 Solution
521 Views
Yuri
NXP Employee
NXP Employee

Please use the non-programmed device (“NP”) for specific options.

OTP can be once programmed.

~Yuri.

View solution in original post

0 Kudos
3 Replies
521 Views
Yuri
NXP Employee
NXP Employee

  According to Table 10 (Start-up Configuration) of the MMPF0100 Datasheet,
VTT mode is not supported neither by default, nor in pre-programmed configs 

(No VTT).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

521 Views
yuuki
Senior Contributor II

Dear Yuri-san,

Thank you for your support.

> VTT mode is not supported neither by default, nor in pre-programmed configs  (No VTT).
=>
We understand it.

In MMPF0100F1, is it possible to overwrite SW4 as VTT mode?

Best Regards,
Yuuki

0 Kudos
522 Views
Yuri
NXP Employee
NXP Employee

Please use the non-programmed device (“NP”) for specific options.

OTP can be once programmed.

~Yuri.

0 Kudos