About UVC camera in AndroidM6.0 for MX6Q-SABRE board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About UVC camera in AndroidM6.0 for MX6Q-SABRE board

跳至解决方案
2,117 次查看
yuuki
Senior Contributor II

Dear all,

We run AndroidM6.0 demo image on MX6Q-SABRE board.
  - Board: MX6Q-SABRE-SD
  - Image: android_M6.0.1_2.0.0_image_6dqpsabresd

We try UVC (USB Video Class) camera input.
However, the USB camera is not recognized.

According to the Release Notes(Rev. M6.0.1_2.0.0, 06/2016), BSP supports Media – USB Camera(Logitech(C250 / E3500)).

Does this pre-build image support the USB Camera?

In addition, camera application is not included in this image.
Would you tell me the available camera application for this image?

Best Regards,
Yuuki

标签 (2)
0 项奖励
回复
1 解答
1,870 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yuuki,

In prebuilt image, USB UVC class camera is supported, you should be able to use on console with gstreamer command..

Please there are some issues regarding camera on SDP board, please check the attached document.

Hope this helps.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,871 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yuuki,

In prebuilt image, USB UVC class camera is supported, you should be able to use on console with gstreamer command..

Please there are some issues regarding camera on SDP board, please check the attached document.

Hope this helps.

0 项奖励
回复
1,870 次查看
yuuki
Senior Contributor II

Dear all, 

I’m sorry to be pressing.
Do you have information about this?

Best Regards,

Yuuki

0 项奖励
回复