About UVC camera in AndroidM6.0 for MX6Q-SABRE board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About UVC camera in AndroidM6.0 for MX6Q-SABRE board

Jump to solution
887 Views
yuuki
Senior Contributor II

Dear all,

We run AndroidM6.0 demo image on MX6Q-SABRE board.
  - Board: MX6Q-SABRE-SD
  - Image: android_M6.0.1_2.0.0_image_6dqpsabresd

We try UVC (USB Video Class) camera input.
However, the USB camera is not recognized.

According to the Release Notes(Rev. M6.0.1_2.0.0, 06/2016), BSP supports Media – USB Camera(Logitech(C250 / E3500)).

Does this pre-build image support the USB Camera?

In addition, camera application is not included in this image.
Would you tell me the available camera application for this image?

Best Regards,
Yuuki

Labels (2)
0 Kudos
1 Solution
641 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yuuki,

In prebuilt image, USB UVC class camera is supported, you should be able to use on console with gstreamer command..

Please there are some issues regarding camera on SDP board, please check the attached document.

Hope this helps.

View solution in original post

0 Kudos
2 Replies
642 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yuuki,

In prebuilt image, USB UVC class camera is supported, you should be able to use on console with gstreamer command..

Please there are some issues regarding camera on SDP board, please check the attached document.

Hope this helps.

0 Kudos
641 Views
yuuki
Senior Contributor II

Dear all, 

I’m sorry to be pressing.
Do you have information about this?

Best Regards,

Yuuki

0 Kudos