About USB VBUS pin termination process of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About USB VBUS pin termination process of i.MX6

Jump to solution
923 Views
yuuki
Senior Contributor II

Dear all,

We use USB_OTG only as Device mode.

In this case I want to detect VBUS by GPIO. (The voltage is converted)
And, the VBUS pin is not used.


Is such use possible?
If it is possible, would you teach the termination process of VBUS pins?


Best Regards,
Yuuki

Labels (1)
Tags (4)
0 Kudos
1 Solution
529 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
530 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
529 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

from i.MX6 side according to USB 2.0 specification USB.org - USB 2.0 Documents

VBUS circuit must limit the inrush current on VBUS. The target maximum droop in the hub

VBUS is 330 mV. This is described in sect.7.2.4.1 Inrush Current Limiting, also

sect.7.2.4.2 Dynamic Detach requires:

"..there must be some minimum capacitance on the device end of the cable to

ensure that the inductive flyback on the open end of the cable does not cause the

voltage on the device end to reverse polarity.

A minimum of 1.0 μF is recommended for bypass across VBUS."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos