About UART communication error by using SDMA in i.MX6SDL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About UART communication error by using SDMA in i.MX6SDL.

ソリューションへジャンプ
1,635件の閲覧回数
keitanagashima
Senior Contributor I


Dear All,

Hello. My customer is testing the UART communication by using SDMA script (uart_2_mcu) on their custom board.

BSP: Linux 3.14.28

Case.1 : HIMASK bit = 1 in SDMAARM_INTRMASK register

- The UART communication error occurred.

- The CHNERR bit = 1 in SDMAARM_EVTERR register.

Case.2 :  HIMASK bit = 0 in SDMAARM_INTRMASK register (<-- Linux BSP default setting)

- The UART can communicate correctly!

- The CHNERR bit = 1 in SDMAARM_EVTERR register.

[Question]

Why is "1" set in CHNERR bit of the SDMAARM_EVTERR register on the channel which used by UART communication (uart_2_mcu script)?

What cause does it notify an error?

Linux BSP set the masked for all channels by default. Is it possible to mask the channel error?

(We worried about whether or not it may mask the error.)

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,435件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments.

1.

> How judge the "pending" or "being serviced" in i.MX6DL?

> I think that SDMA checks the EP register. 

  Yes.

2.

> Why is it possible to mask the channels in the INTRMASK regardless
> of channel error occurrence?

  This is possible if data loss is not a problem for an application.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,435件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I hope the following helps.

https://community.nxp.com/message/507608#comment-507608

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,435件の閲覧回数
keitanagashima
Senior Contributor I

Hi Yuri,

Thank you for your reply.

> The SDMA has ability to "warn the ARM platform when an incoming DMA request was

>detected and it triggers a channel that is already pending or being serviced." SDMAARM_EVTERR is used for it.

How judge the "pending" or "being serviced" in i.MX6DL?

I think that SDMA checks the EP register.

>If such kind of events are needed to be served / tracked, it is required to unmask (enable) corresponding events

>in SDMAARM_INTRMASK. Generally it is possible to mask (disable) some channels in the INTRMASK - in order
>to skip possible overflow of data for some active channel.

I couldn't understand well.

You said "Generally it is possible to mask (disable) some channels in the INTRMASK - in order to skip possible overflow of data for some active channel."

Why is it possible to mask the channels in the INTRMASK regardless of channel error occurrence?

Best Regards,

Keita

0 件の賞賛
返信
1,436件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments.

1.

> How judge the "pending" or "being serviced" in i.MX6DL?

> I think that SDMA checks the EP register. 

  Yes.

2.

> Why is it possible to mask the channels in the INTRMASK regardless
> of channel error occurrence?

  This is possible if data loss is not a problem for an application.

Regards,

Yuri.

0 件の賞賛
返信