About Table 9-11 Re-enabling the power in i.MX 7Dual Applications Processor Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Table 9-11 Re-enabling the power in i.MX 7Dual Applications Processor Reference Manual

Jump to solution
728 Views
goto11
Contributor III

Hello,

Step 7 has a description of DDR Remove the core reset.
I thought this control would control the DDRC_CORE_RST Field.
However, at the URL below, I found that there is a PATCH that controls DDRC_CORE_RST Field and DDRC_PRST Field.
Do I have to reflect the processing described in PATCH in the source code?

http://u-boot.10912.n7.nabble.com/PATCH-ARM-imx-ddr-Add-missing-PHY-reset-td414340.html

best regards
Goto

0 Kudos
Reply
1 Solution
692 Views
joanxie
NXP TechSupport
NXP TechSupport

table 9-11 is for Power Removal, the patch is for Re-enabling the power, if you need to re-enable the power, you need to use the patch

View solution in original post

0 Kudos
Reply
3 Replies
720 Views
joanxie
NXP TechSupport
NXP TechSupport

where is step7? could you share with me?"I thought this control would control the DDRC_CORE_RST Field." what "this control" do you mean?

0 Kudos
Reply
716 Views
goto11
Contributor III

This is the leftmost Step column in Table 9-11.
I thought that the following Description can be processed by setting DDRC_CORE_RST Field.

Excerpt from Step 7 Description
Remove the core reset core_ddrc_rstn = 1’b1
aresetn_n = 1’b1

best regards
Goto

0 Kudos
Reply
693 Views
joanxie
NXP TechSupport
NXP TechSupport

table 9-11 is for Power Removal, the patch is for Re-enabling the power, if you need to re-enable the power, you need to use the patch

0 Kudos
Reply