Hello,
Please tell me the correspondence between Full Speed Phase Selection and Full Speed Delay Selection with QSPI_WMPR [DDRSMP].
As an example, please tell us about two cases.
What is QSPI_WMPR [DDRSMP] set when Full Speed Phase Selection is "1" and Full Speed Delay Selection is "0"?
What is QSPI_WMPR [DDRSMP] set when Full Speed Phase Selection is "1" and Full Speed Delay Selection"1"?
Regards,
Goto
Hi Goto
parameter QSPI_WMPR [DDRSMP] is set based on timings used qspi-nor part (can be found
in its datasheet), sect.10.2.10.2 Input timing in DDR mode with internal sampling
i.MX 7Dual Applications Processor Reference Manual
and sect.4.10.11.2 DDR Mode i.MX 7Dual Family of Applications Processors Datasheet
Best regards
igor
Hello,
Can you tell me the value in the "?" Column in the table below?
Full Speed Phase Selection | 0 | 1 | 0 | 1
_______________________________________________________________
Full Speed Delay Selection | 0 | 0 | 1 | 1
_______________________________________________________________
QSPI_WMPR [DDRSMP] | ? | ? | ? | ?
Regards,
Goto
Hello,
Table 6-50 of i.MX 7 Dual Reference Manual (page 1236) of the i.MX 7 Dual Applications Processor Reference Manual.
Can you tell me the value in the "?" Column in the table below?
Full Speed Phase Selection | 0 | 1 | 0 | 1
_______________________________________________________________
Full Speed Delay Selection | 0 | 0 | 1 | 1
_______________________________________________________________
QSPI_SMPR [DDRSMP] | ? | ? | ? | ?
Regards,
Goto
>Can you tell me the value in the "?" Column in the table below?
these parameters should be set based on qspi-nor flash datasheet values.
In particular for MX25L51245GZ2I-10G part used in i.MX7D Sabre SD board
there is example in mfg tool package, file qspi-nor-macronix-mx25l51245g-config
Best regards
igor