Dear Sir or Madam,
Hello.I have a question about CSI_PIXCLK of Gated Clock Mode Timing in i.MX6SL.
Refer to "4.10.2.0.1 Gated Clock Mode Timing" in IMX6SLCEC_Rev.3.
There is below description.
"The pixel clock, CSI_PIXCLK (PIXCLK), is valid as long as HSYNC is asserted."
Is it possible to stop CSI_PIXCLK (PIXCLK) from external device, as long as HSYNC is de-asserted?
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita
yes possible. Timing is similar to non-gated mode, RM shows it :
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
yes possible. Timing is similar to non-gated mode, RM shows it :
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------