About STOP MODE of PMU with i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About STOP MODE of PMU with i.MX6UL

Jump to solution
597 Views
yuuki
Senior Contributor II

Dear all,

I have a question about STOP MODE of PMU of MX6UL.

I refer to STOP_MODE_CONFIG Field of Miscellaneous Register 0 (PMU_MISC0) in MX6UL Refrence Manual.

The 0x11 setting shows "STOP (very lower power)-Analog regulators are OFF".

STOP_MODE_CONFIG Field.png

However, in Table 10-3. STOP mode configuration, I think that explanation of STOP_MODE_CONFIG is reverse.

Table 10-3.png

I understand that explanation of STOP_MODE_CONFIG Field is right.
Is my understanding right?

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Solution
518 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Table 10-3 (STOP mode configuration) is not fully correct regarding

column names :

instead of “STOP_MODE_CONFIG=0” – should be “Analog regulators are OFF”

instead of “STOP_MODE_CONFIG=1” – should be “Analog regulators are ON”.


Have a great day,
Yuri
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
519 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Table 10-3 (STOP mode configuration) is not fully correct regarding

column names :

instead of “STOP_MODE_CONFIG=0” – should be “Analog regulators are OFF”

instead of “STOP_MODE_CONFIG=1” – should be “Analog regulators are ON”.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos