About SSI supporting format (24bit 3byte) in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About SSI supporting format (24bit 3byte) in i.MX6DQ.

ソリューションへジャンプ
1,420件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. Please see the below community.

snd_pcm_format_s24_3le and the SSI driver 

There is description of "SNDRV_PCM_FMTBIT_S24_3LE(24-bit data format without padding) is not supporting"

Is this the meaning not to be supporting by hardware?

Or, If the software can be modified, is it possible to support the format?

Best Regards,

Keita

ラベル(4)
0 件の賞賛
返信
1 解決策
1,249件の閲覧回数
art
NXP Employee
NXP Employee

The 24-bit data without padding format is supported by SSI in hardware. Not sure about Linux BSP driver. Some software modifications may be required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,250件の閲覧回数
art
NXP Employee
NXP Employee

The 24-bit data without padding format is supported by SSI in hardware. Not sure about Linux BSP driver. Some software modifications may be required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信