About SSI supporting format (24bit 3byte) in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About SSI supporting format (24bit 3byte) in i.MX6DQ.

跳至解决方案
1,586 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello. Please see the below community.

snd_pcm_format_s24_3le and the SSI driver 

There is description of "SNDRV_PCM_FMTBIT_S24_3LE(24-bit data format without padding) is not supporting"

Is this the meaning not to be supporting by hardware?

Or, If the software can be modified, is it possible to support the format?

Best Regards,

Keita

标签 (4)
0 项奖励
回复
1 解答
1,415 次查看
art
NXP Employee
NXP Employee

The 24-bit data without padding format is supported by SSI in hardware. Not sure about Linux BSP driver. Some software modifications may be required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,416 次查看
art
NXP Employee
NXP Employee

The 24-bit data without padding format is supported by SSI in hardware. Not sure about Linux BSP driver. Some software modifications may be required.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复