About SSI(I2S master mode problem),we used a chip pcm5100ADC on IMX6 solo board, it need I2S be master mode. It always failed. we found it seems have data without clk.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About SSI(I2S master mode problem),we used a chip pcm5100ADC on IMX6 solo board, it need I2S be master mode. It always failed. we found it seems have data without clk.

4,246 Views
huaiguangliu
Contributor I
0 Kudos
Reply
20 Replies

2,653 Views
zh597588308
Contributor I

hi

     could you tell me your e-mail? I have the same question.

0 Kudos
Reply

2,656 Views
saurabh206
Senior Contributor III

Hi

Please change SND_SOC_CLOCK_IN to SND_SOC_CLOCK_OUT.

snd_soc_dai_set_sysclk(cpu_dai, IMX_SSP_SYS_CLK, 0, SND_SOC_CLOCK_OUT);

You should get your playback.

Thanks

Saurabh

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

I have tried this but still failed. Now problem is here have any signal in BCK and LRCK. 

I can't see any init ssi_clk code in clock.c I doubt SSI module have no clock input,

I added some code in clock.c but it not work . Please see below  code. Did it right?

clk_set_parent(&ssi1_clk, &pll4_audio_main_clk);

    clk_enable(&pll4_audio_main_clk);

    rate = clk_round_rate(ssi1_clk, 12288000);

    clk_set_rate(&ssi1_clk,rate);

Thanks!

0 Kudos
Reply

2,656 Views
saurabh206
Senior Contributor III

Have you changed the

static struct clk ssi1_clk

for correct .parent ?

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

No.I didn't.

Do you mean it will default use .parent?

It is strange when we play .wav , here hvae data siganl without any clk signal in ssi bus.

0 Kudos
Reply

2,656 Views
saurabh206
Senior Contributor III

You need correct two things

snd_soc_dai_set_sysclk(cpu_dai, IMX_SSP_SYS_CLK, 0, SND_SOC_CLOCK_OUT);

and

static struct clk ssi1_clk = {

    __INIT_CLK_DEBUG(ssi1_clk)

    .parent = &pll4_audio_main_clk,

Please correct it and verify your audio.

Thanks

Saurabh

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

Do I need keep below code?

clk_set_parent(&ssi1_clk, &pll4_audio_main_clk);

    clk_enable(&pll4_audio_main_clk);

    rate = clk_round_rate(ssi1_clk, 12288000);

    clk_set_rate(&ssi1_clk,rate);

thanks!

0 Kudos
Reply

2,656 Views
saurabh206
Senior Contributor III

yes

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

our bsp version is imx_kk4.4.2_1.0.0-ga

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

Today we found we use code imx6q_add_imx_ssi(1, &mx6_sabresd_ssi_pdata) that in fact we used ssi2, and we change code to below but still failed.

clk_set_parent(&ssi2_clk, &pll4_audio_main_clk);

    clk_enable(&pll4_audio_main_clk);

    rate = clk_round_rate(ssi2_clk, 12288000);

    clk_set_rate(&ssi2_clk,rate);

0 Kudos
Reply

2,656 Views
liu_jialu
Contributor III

have you solve the ssi2_clk problem? i meet the same problem, cat't get 12288000, but get 86016000 from /sys/kernel/debug/clock/osc_clk/pll4_audio_main_clk/ssi2_clk/rate

0 Kudos
Reply

2,656 Views
Jacky_Song
Contributor III

hi liu:

     i got same issue with SSI master mode. and i got no bclk or fsclk too. have you work out this problem?

0 Kudos
Reply

2,656 Views
liu_jialu
Contributor III

have you solve the ssi2_clk problem? i meet the same problem, cat't get 12288000, but get 86016000 from /sys/kernel/debug/clock/osc_clk/pll4_audio_main_clk/ssi2_clk/rate

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

unfortunnately, It still work failed.

DAC mclk is from clko(we can get and about is 24MHZ). and his parent is clko2_clk.

From datasheet we know we can set his parent is pll4_audio_main_clk. In this case. DAC mclk disappeared.

So can we doubt pll4_audio_main_clk have no clock?

Do we need set code clk_set_parent( &pll4_audio_main_clk,osc_clk)?

After I test it and still failed :smileysad:.

Correct:I make  a mistake, pll4_audio_main_clk have clk outout.Please ignore up  content..

Do you have any suggestions?

below is SSI register settings from trace when we start play .wav file.

tinyplay //data/PROmp15.wav -D 0

[Jenny DBG~~]imx_hifi_hw_params params_rate:44100[Jenny DBG~~]imx_ssi_set_dai_tdm_slot  SSI_STCCR = 0x40100

[Jenny DBG~~]imx_ssi_set_dai_fmt  SSI_STCR = 0x3ed scr=0x130

[Jenny DBG~~]snd_soc_dai_set_clkdiv cpu_dai done!!!

[Jenny DBG~~]imx_ssi_hw_paramschannels = 2 scr=0x1b8 SSI_STCCR = 0x4e104

Playing sample: 2 ch, 44100 hz, 16 bit

[Jenny DBG~~]imx_ssi_trigger  SSI_SCR = 0x1bb

[Jenny DBG~~]imx_ssi_trigger  SSI_SCR = 0x1b8

Thanks!

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

I doubt bsp didn't init ssi clock in clock.c of arch/arm/mach-mx6/

0 Kudos
Reply

2,656 Views
saurabh206
Senior Contributor III

Hi Liu

Which BSP and kernel you are using?

What modification do you have made?

Default BSP doesn't support SSI master.

Thanks

Saurabh

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

kernel 3.0.35,mach-mx6,board-mx6q-sabresd.

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

We follow datasheet <i.MX 6Solo/6DualLite Applications Processor Reference Manual>  SSI I2S master mode to set SSI reg. .  In pcm51xx dai driver call cpu_dai to set format and clk.

0 Kudos
Reply

2,656 Views
saurabh206
Senior Contributor III

Hi

Have you changed platform driver from "SND_SOC_DAIFMT_CBM_CFM" to "SND_SOC_DAIFMT_CBS_CFS"?

Have you set MCLK and SSI clock?

0 Kudos
Reply

2,656 Views
huaiguangliu
Contributor I

We have set and can get MCLK in pcm5100 DAC.

in pin DIN and SCK we can get signal ,BCk and LRCK have nothing.

Please see our settings:

dai_format = SND_SOC_DAIFMT_I2S | SND_SOC_DAIFMT_NB_IF |

        SND_SOC_DAIFMT_CBS_CFS;

    ssi_mode->flags |= IMX_SSI_SYN;

    /* set cpu DAI configuration */

    ret = snd_soc_dai_set_fmt(cpu_dai, dai_format);

    if (ret < 0){

        pr_err("hw_params snd_soc_dai_set_fmt cpu_dai failed : %d\n", ret);

        return ret;

    }

    /* set the SSI system clock as input (unused) */

    

    snd_soc_dai_set_sysclk(cpu_dai, IMX_SSP_SYS_CLK, 0, SND_SOC_CLOCK_IN);

    snd_soc_dai_set_clkdiv(cpu_dai, IMX_SSI_TX_DIV_PM, 4);

    snd_soc_dai_set_clkdiv(cpu_dai, IMX_SSI_TX_DIV_2, 1);

    snd_soc_dai_set_clkdiv(cpu_dai, IMX_SSI_TX_DIV_PSR, 0);

0 Kudos
Reply