About SPI I/F of i.MX 6Dual.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About SPI I/F of i.MX 6Dual.

跳至解决方案
837 次查看
takashitakahash
Contributor III

Dear community.

Our customer has question below.

About the SPI interface of  i.MX6Dual ,
Is it possible to toggle the burst transfer in Master mode every time like 512 bytes, 496 bytes, 512 bytes, 496 bytes, and so on?

FIFO read / write uses DMA.

标签 (1)
0 项奖励
1 解答
714 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

I am afraid not as BURST_LENGTH register ECSPIx_CONREG

should be configured properly every time for particular burst size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
715 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

I am afraid not as BURST_LENGTH register ECSPIx_CONREG

should be configured properly every time for particular burst size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励