About SPI I/F of i.MX 6Dual.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About SPI I/F of i.MX 6Dual.

ソリューションへジャンプ
855件の閲覧回数
takashitakahash
Contributor III

Dear community.

Our customer has question below.

About the SPI interface of  i.MX6Dual ,
Is it possible to toggle the burst transfer in Master mode every time like 512 bytes, 496 bytes, 512 bytes, 496 bytes, and so on?

FIFO read / write uses DMA.

ラベル(1)
0 件の賞賛
1 解決策
732件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

I am afraid not as BURST_LENGTH register ECSPIx_CONREG

should be configured properly every time for particular burst size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
733件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

I am afraid not as BURST_LENGTH register ECSPIx_CONREG

should be configured properly every time for particular burst size.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛