About RGB-selection of SCART terminal in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About RGB-selection of SCART terminal in i.MX6DQ.

跳至解决方案
1,247 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Is it possible to output the RGB-selection signal in i.MX6DQ's IPU?

Refer to below link and 16 pin.

SCART - Wikipedia, the free encyclopedia

=======

Pin 16 Blanking signal up

RGB-selection voltage up

0 - 0.4 V --> composite

1 - 3 V --> RGB

=======

(My customer would like to use the external IC to overlay the two video "RGB and composite".)

Best Regards,

Keita

标签 (4)
0 项奖励
回复
1 解答
1,171 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

unfortunately i.MX6DQ's IPU can not produce

such kind of signal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,172 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

unfortunately i.MX6DQ's IPU can not produce

such kind of signal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,171 次查看
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your prompt reply!

Best Regards,

Keita

0 项奖励
回复