Dear all,
We refer to Description in REGx_ADJ field of PMU_REG_CORE register.
IMX6SDLRM.pdf:
- 51.7.1 Digital Regulator Core Register (PMU_REG_CORE)(P.4522)
REGx_ADJ=0000 is "No adjustment".
In what kind of case is setting of REGx_ADJ=0000 used?
May I have advice?
Best Regards,
Yuuki
Solved! Go to Solution.
Hi yuuki
REGx_ADJ=0000 means default, as
IMX6SDLRM p.4517 describes:
The target voltages of these regulators are all reset to 1.1 V on startup.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yuuki
REGx_ADJ=0000 means default, as
IMX6SDLRM p.4517 describes:
The target voltages of these regulators are all reset to 1.1 V on startup.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------