About QuadSPI configuration parameter description

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About QuadSPI configuration parameter description

跳至解决方案
990 次查看
eishishibusawa
Contributor III

Dear Sir

 

I refer to the IMX6ULLRM Rev.1.

I want to confirm the value in Table 8-23.

 

Name : Hold Delay

Value : QSPI1 B : QSPI1 A = 01 : Disable : Enable

Q1.

Is this value a binary number?

(Value 01 <- 2b01 ?)

 

Name : Serial Clock Frequency

Value : Clock = 06 : 99 MHz (only SDR mode)

Q2.

Is this value a decimal number?

 

Name : Mode of operation of serial Flash

Value : Mode = 01 : Single

Q3.

Is this value a decimal number?

 

Best Regards,

Eishi SHIBUSAWA

 

标签 (1)
0 项奖励
回复
1 解答
929 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

1.  yes

2.  yes

3.  yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
930 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

1.  yes

2.  yes

3.  yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复