About QUIRK_BROKEN_AUTO_CMD23 in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About QUIRK_BROKEN_AUTO_CMD23 in i.MX6DQ.

ソリューションへジャンプ
1,204件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about changing "ChunkSize" by CMD23.

My customer wants to change the ChunkSize of eMMC by CMD23 to reduce the erase count in SLC area.

And, they are using BSP L3.0.35_4.1.0.

But, the NXP source code doesn't use auto cmd23 temporarily.

Refer to below thread.

linux-2.6-imx.git - Freescale i.MX Linux Tree

+ if (cpu_is_mx6())

+ host->quirks2 |= SDHCI_QUIRK_BROKEN_AUTO_CMD23,

+

Next, refer to latest BSP(L3.14.52_1.1.0).

The above patch wasn't found.

linux-2.6-imx.git - Freescale i.MX Linux Tree

[Question]

Q1.

Why does NXP prohibit the use of this code?

(I didn't understand the description of ENGR00178290-2 well...)

-----

if (cpu_is_mx6())

             host->quirks2 |= SDHCI_QUIRK_BROKEN_AUTO_CMD23;

-----

Q2.

What influence is there if the user uses this code?

Best Regards,

Keita

ラベル(4)
0 件の賞賛
返信
1 解決策
931件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

usage CMD23 is optional accrding to sd/emmc specifications and it is

not supported by i.MX6 uSDHC according to Table 67-5 "Commands for MMC/SD/SDIO

Cards" i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
931件の閲覧回数
keitanagashima
Senior Contributor I

Do you have any update?

Best Regards,

Keita

0 件の賞賛
返信
932件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

usage CMD23 is optional accrding to sd/emmc specifications and it is

not supported by i.MX6 uSDHC according to Table 67-5 "Commands for MMC/SD/SDIO

Cards" i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
931件の閲覧回数
keitanagashima
Senior Contributor I

Dear Igor,

Sorry. Let me check again.

> it is not supported by i.MX6 uSDHC according to Table 67-5 "Commands for MMC/SD/SDIO

> Cards" i.MX6DQ Reference Manual (rev.3  7/2015)

What is your meaning of "not supported"?

Which is right understanding?

ex.1) uSDHC doesn't send the CMD23 even if it tries to send CMD23.

ex.2) NXP didn't test the CMD23. So, NXP doesn't know whether or not it is possible to send CMD23.

Best Regards,

Keita

0 件の賞賛
返信
931件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

uSDHC doesn't send the CMD23, it even does not try to send CMD23.

Best regards

igor

0 件の賞賛
返信