About PWM software reset time in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About PWM software reset time in i.MX6DQ.

Jump to solution
928 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. I have a question about PWM software reset time in i.MX6DQ.

Refer to 51.7.1 PWM Control Register (PWMx_PWMCR) in i.MX6DQRM(Rev.3).

"SWR bit" : PWM is reset when this bit is set to 1. It is a self clearing bit.

How long the reset period from SWR=1 to SWR=0 at the worst time?

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
860 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Keita Nagashima,

I couldn’t find this value on the documentation.

However, if you see section 51.7.5 (PWMx_PWMPR) of the i.MX6 DQ Reference Manual (rev. 3) the lower limit of the PWM is two clock cycles so I would expect the software reset to take around two clock cycles to reset the registers.

View solution in original post

0 Kudos
Reply
1 Reply
861 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Keita Nagashima,

I couldn’t find this value on the documentation.

However, if you see section 51.7.5 (PWMx_PWMPR) of the i.MX6 DQ Reference Manual (rev. 3) the lower limit of the PWM is two clock cycles so I would expect the software reset to take around two clock cycles to reset the registers.

0 Kudos
Reply