Dear All,
MC32PF3000A4EP
Programming Options : 4 (i.MX 6 Series with DDR3)
In above ”A4” programming, SW2 output 3.3V (+-6%).
But, the VDD_HIGH, NVCC33_IO: 2.8Vmin - 3.3Vmax were defined by i.MX6SL.
Is it possible to use the MC32PF3000A4EP for i.MX6SL?
Best Regards,
Keita
已解决! 转到解答。
Hello,
App note AN5113 (Powering an i.MX 6SL Based System Using
the PF3000 PMIC) provides recommended configuration in Table 2 (PF3000 + i.MX 6SL
Power Tree), assuming LPDDR2 (preprogrammed A5 configuration).
http://cache.nxp.com/files/analog/doc/app_note/AN5113.pdf
Nevertheless, considering the A4 case regarding 3.3V, note,
maximum GPIO and VDD_HIGH_IN supply voltage (Absolute Maximum Ratings) is 3.6V ; this
allows to decrease the SW2 output below 3.3V as soon as possible after boot for reliable
operation.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
App note AN5113 (Powering an i.MX 6SL Based System Using
the PF3000 PMIC) provides recommended configuration in Table 2 (PF3000 + i.MX 6SL
Power Tree), assuming LPDDR2 (preprogrammed A5 configuration).
http://cache.nxp.com/files/analog/doc/app_note/AN5113.pdf
Nevertheless, considering the A4 case regarding 3.3V, note,
maximum GPIO and VDD_HIGH_IN supply voltage (Absolute Maximum Ratings) is 3.6V ; this
allows to decrease the SW2 output below 3.3V as soon as possible after boot for reliable
operation.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Thank you for your reply.
> App note AN5113 (Powering an i.MX 6SL Based System Using
>the PF3000 PMIC) provides recommended configuration in Table 2 (PF3000 + i.MX 6SL
>Power Tree), assuming LPDDR2 (preprogrammed A5 configuration).
OK. Thank you.
But, the target is DDR3(1.5V).
> Nevertheless, considering the A4 case regarding 3.3V, note,
>maximum GPIO and VDD_HIGH_IN supply voltage (Absolute Maximum Ratings) is 3.6V ; this
>allows to decrease the SW2 output below 3.3V as soon as possible after boot for reliable
>operation.
OK. I got it.
Best Regards,
Keita
Hi Keita,
Yes it is officially supported, see this https://www.nxp.com/webapp/search.partparamdetail.framework?PART_NUMBER=MC32PF3000A4EP
Michal
Dear Michal,
Thank you for your prompt reply.
SW2 output 3.3V (+-6%) : Max 3.498V!
The voltage outs of operating range in i.MX6SL.
Is it possible to guarantee the voltage (3.498V) on VDD_HIGH, NVCC33_IO of i.MX6SL?
Best Regards,
Keita