About ONOFFpin input signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ONOFFpin input signal

ソリューションへジャンプ
1,808件の閲覧回数
goto11
Contributor III

hello,Community

In order to transition to the ON state, when (debounce time) + (ON_TIME) has elapsed, the PMIC_ON_REQ signal will be output high.
If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
Or do you have to keep ONOFFpin low during the ON_TIME period?

(See attachment)

best regards

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,721件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
>Or do you have to keep ONOFFpin low during the ON_TIME period?

necessary to keep ONOFFpin low during the ON_TIME period.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,722件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Goto

>If the ONOFFpin low level signal exceeds the debounce time, will it transition to the ON state?
>Or do you have to keep ONOFFpin low during the ON_TIME period?

necessary to keep ONOFFpin low during the ON_TIME period.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信