About OMX Player in AndroidM6.0.1_2.1.0 for i.MX6Q-SABRE-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About OMX Player in AndroidM6.0.1_2.1.0 for i.MX6Q-SABRE-SDB

769 Views
yuuki
Senior Contributor II

Daer all,

We run AndroidM6.0.1_2.1.0 BSP on i.MX6Quad SABRE-SDB.

According to the following release note, Stagefright is used as default media framework.
And the OMXPlayer is only used for RTP/UDP streaming.

- i.MX_Android_Extended_Codec_Release_Notes.pdf

The OMXPlayer was used in Android4 .4.3.

We want to use by default OMXPlayer on AndroidM6.0.1_2 .1.0.

Can we use by default OMXPlayer?
Would you tell me the method if it is possible?

Best Regards,
Yuuki

Labels (2)
0 Kudos
3 Replies

518 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi yuuki,

Codecs that have license restriction are provided in separate packages.For Install the OMXPlayer as default media framework you need to get the sources packages and rebuild the bsp. To obtain the mentioned package, you should contact with Freescale local FAE or Marketing office.

Regards

 

0 Kudos

518 Views
yuuki
Senior Contributor II

Dear Bio_TICFSL-san,

AndroidKK4 .4.3 needed OMXPlayer package.

However, we understand that AndroidM6.0.1_2 .1.0 has already included OMXPlayer.
"Used Stagefright as the default media framework rather than OMXPlayer. OMXPlayer is only used for RTP/UDP streaming."

Is my understanding wrong?
Does OMX player package for AndroidM6.0.1_2 .1.0 exist separately?

Best Regards,
Yuuki

0 Kudos

518 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Yuuki,

Correct!, M6.0.1_2.1.0 does not provide source of omxplayer/wfdsink separately, all source is included in one package. and need to be provided via Marketing.

Regards

0 Kudos