Dear All,
Hello.
Refer to description of "OEA" bit in EIM_CSnRCR1 register on IMX6DQRM (Rev.3).
"In muxed mode OE assertion occurs (OEA + RADVN + RADVA + ADH +1) EIM clock cycles from start of access."
But, my customer measured the OEA signal on their custom board.
The result was (OEA + RADVN + RADVA + ADH + BCD + BCS +1).
On the other hand, refer to description of "RADVN" bit.
"ADV negation occurs according to the following formula:
(RADVN + RADVA + BCD + BCS + 1) EIM clock cycles from start of access."
[Question]
Is the following formula right?
"OE assertion = OEA + RADVN + RADVA + ADH + BCD + BCS +1"
i.e) is the description of Reference Manual typo?
Best Regards,
Keita
Hello,
Yes, the BCD should be taken into account ; please refer
to definition of parameter WE10 (Clock rise to EIM_OE_B valid)
in the Datasheet :
min = -0.5 × t × (k+1) - 1.25 ;
max = -0.5 × t × (k+1) + 2.25,
where k represents register setting BCD value.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
------------------------------------------------------------------------------
Hi Yuri,
Thank you for your reply.
Let me confirm again.
The "BCS" parameter should be considered, isn't it?
Best Regards,
Keita