About ODT setting for DRAM_SDQS0 and DRAM_SDQS1 of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ODT setting for DRAM_SDQS0 and DRAM_SDQS1 of i.MX6Solo

Jump to solution
1,524 Views
yuuki
Senior Contributor II

Dear all,

I want to set ODT for DRAM_SDQS0 and DRAM_SDQS1.
However, ODT[10:8] field of the IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQSx_P register is Read Only.

Can we set OTD for DRAM_SDQS0 and DRAM_SDQS1?

If it is possible, would you tell me the register name and field?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
1,277 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Look at https://community.nxp.com/message/863150 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,278 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Look at https://community.nxp.com/message/863150 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply