About ODT setting for DQS in MX6DL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ODT setting for DQS in MX6DL.

ソリューションへジャンプ
1,081件の閲覧回数
keitanagashima
Senior Contributor I

Hi.

I have a question about ODT setting for DQS in i.MX6SDL.

First, refer to 36.4.358 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS0_P) in IMX6DQRM_Rev.1.

===

On Die Termination Field

Select one of next values for pad: DRAM_SDQS0.

000 DISABLED— Disabled

001 120_OHM— 120 Ohm ODT

010 60_OHM— 60 Ohm ODT

011 40_OHM— 40 Ohm ODT

100 30_OHM— 30 Ohm ODT

101 24_OHM— 24 Ohm ODT

110 20_OHM— 20 Ohm ODT

111 17_OHM— 17 Ohm ODT

===

Next, refer 37.4.299 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_DRAM_SDQS0_P) in IMX6SDLRM_Rev.1.

===

On Die Termination Field

Read Only Field

The value of this field is fixed and cannot be changed.

000 DISABLED— Disabled

===

[Question]

I seemed that SDQS can't set ODT in i.MX6SDL.

Is there any way of setting ODT of SDQS or Not?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
911件の閲覧回数
Yuri
NXP Employee
NXP Employee

Generally it is recommended to use only MMDC_MPODTCTRL register to configure ODT.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
912件の閲覧回数
Yuri
NXP Employee
NXP Employee

Generally it is recommended to use only MMDC_MPODTCTRL register to configure ODT.

0 件の賞賛
返信