About OCRAM_S in i.MX7Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About OCRAM_S in i.MX7Solo

Jump to solution
1,283 Views
yuuki
Senior Contributor II

Dear all,

i.MX7Solo has some OCRAM areas.

 - 0094_0000 - 0094_7FFF:  32KB / OCRAM_PXP
 - 0092_0000 - 0093_FFFF: 128KB / OCRAM_GP
 - 0090_0000 - 0091_FFFF: 128KB / OCRAM 128KB
 - 0018_0000 - 0018_7FFF:  32KB / OCRAM_S

I understood that OCRAM_PXP, OCRAM_GP and OCRAM 128KB could be used as Free Area.

(Reserved 46KB is excluded)

Can OCRAM_S be used as Free Area?

Best Regards,
Yuuki

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,016 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The OCRAM parts are available for customer use when the corresponding block is not used :

- on a part where the EPDC is not available(ie disabled) the EPDC OCRAM (for i.MX7D) is free for applications  ;

- the memory, attached to the PXP, is user accessible if the PXP is not in use.

  On i.MX7D/S, the boot vector for the M4 core is located at the start of the OCRAM_S, so it may be used for

other purposes, when no applications for CM4.

https://community.nxp.com/docs/DOC-331940 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,017 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The OCRAM parts are available for customer use when the corresponding block is not used :

- on a part where the EPDC is not available(ie disabled) the EPDC OCRAM (for i.MX7D) is free for applications  ;

- the memory, attached to the PXP, is user accessible if the PXP is not in use.

  On i.MX7D/S, the boot vector for the M4 core is located at the start of the OCRAM_S, so it may be used for

other purposes, when no applications for CM4.

https://community.nxp.com/docs/DOC-331940 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,016 Views
yuuki
Senior Contributor II

Yuri

Dear Yuri-san,

Thank you for yoru information.

I clicked the URL.

However, I cannot access this URL.

Best Regards,

Yuuki

0 Kudos
Reply
1,016 Views
Yuri
NXP Employee
NXP Employee

Hello Yuuki-san !

  Sorry, it was internal link. Please refer to the note in section 3.1

(On-chip memory view from each ARM core on the i.MX 7Dual/7Solo)

of app note AN5317.

http://www.nxp.com/assets/documents/data/en/application-notes/AN5317.pdf 

Regards,

Yuri.