Hi, I am have a question about the Parallel CSI module, hope here can get answer, thank you!
When MPU is running in Non-Gated Clock Mode, because the HSYNC signal will be ignored,
How know a line the number of pixels, it is possible using the clock edge to latched data; if so, in this Parallel_CSI_TX side, the pixel data of a line can many discontinuous clock cycles to send out ?
2,The Data_EN signal in the Parallel_CSI_RX is necessary? The figure 19 on page758 of document (IMX6ULLRM.pdf), Here is no use this Data_EN signal.
3, When sending a line of pixels, is the need for a continuous clock to send a line, or send a line of pixels can be discontinuous .
Please see below the figure, thank you!