About MMDC1_MDCFG0 "tXP" bit in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MMDC1_MDCFG0 "tXP" bit in i.MX6DQ.

Jump to solution
481 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have a question about setting the tXP bit.

tXP bit value must set more than 1 clock than tCKE from DDR3 SDRAM Specification JESD79-3E.

If "tXP bit value" > "tCKE bit value", does it work according to the setting?

Or, is it automatically calibrated?

Best Regards,

Keita

Labels (3)
0 Kudos
1 Solution
404 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

>If "tXP bit value" > "tCKE bit value", does it work according to the setting?

Yes.

> is it automatically calibrated?

No, it is not calibrated automatically.

Best regards

igor
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
405 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

>If "tXP bit value" > "tCKE bit value", does it work according to the setting?

Yes.

> is it automatically calibrated?

No, it is not calibrated automatically.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos