About MIPI interface of imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MIPI interface of imx6

Jump to solution
900 Views
okamotosatoshi
Contributor IV

Hi There,

I want to check for IMX6.
Unused MIPI recommends "Leave unconnected".

Hardware Development Guide for i.MX 6DualPlus/6QuadPlus, 6Dual/6Quad and i.MX 6Solo/6DualLite Applications Processors
2.8 Unused analog interfaces

Is this due to shutting down the PHY?

We are considering whether termination is necessary when the camera is not in use.
Is it possible to terminate (for internal IMX6) MIPI CSI?
Do I have to terminate externally?

Best regards
- satoshi

Labels (4)
0 Kudos
Reply
1 Solution
746 Views
Yuri
NXP Employee
NXP Employee

Hello

  Please just follow recommendations of the Hardware Development Guide :

no need for termination of the mentioned signals.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

0 Kudos
Reply
2 Replies
747 Views
Yuri
NXP Employee
NXP Employee

Hello

  Please just follow recommendations of the Hardware Development Guide :

no need for termination of the mentioned signals.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply
746 Views
okamotosatoshi
Contributor IV

Hi, Yuri

Thank you for your advice.
We will consider countermeasures against noise when not in use.

Very Thanks.

Best regards
- satoshi

0 Kudos
Reply