I looked for the detailed information of MCIMX-LVDS1.
However, I was able to find neither a datasheet nor a schematic.
I would like to know the following information.
- Liquid crystal maker
- Part Number
- Viewing angle
- I/F specification (pin assignment, timing etc.)
Best Regards,
Solved! Go to Solution.
Hi yuuki,
Sorry for delay reply. Yes, the MCIMX-LVDS1 has a touch-panel controller. It has a HanStar part number (HSD100PXN1) on it. They use the Galaxy Touch device .And the touch screen is included with the LVDS1 display. Hope this can help you.
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The only functional part of the MCIMX-LVDS1 module is the HSD100PXN1 LVDS LCD +
capacitive touch screen panel by HannStar:
http://www.hannstar.com/Common.aspx?mid=198&tmid=3&modid=4
For the detailed information on it, please contact them directly:
http://www.hannstar.com/Common.aspx?mid=231&tmid=93&modid=1
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi yuuki,
We are sorry for getting back to you so late. About MCIMX-LVDS1 I only have information on freescale official website, the link is http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&tab=Buy_Parametric_Tab&fromS....
The LVDS interface design you can refer to the Schematics of every boards on different processors.
Hope this can help you.
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Dan-san,
Thank you for the reply.
I think that MCIMX-LVDS1 has a touch-panel controller.
I want the information of maker and a part number of this touch-panel controller.
Would you let me know, if you have these informations?
I found MAX11801 on the SABRE-SDB board.
However, this is a Resistive membrane type touch panel.
I understand that MCIMX-LVDS1 has a controller of Electrostatic capacitance type touch panel.
Best Regards,
Hi yuuki,
Sorry for delay reply. Yes, the MCIMX-LVDS1 has a touch-panel controller. It has a HanStar part number (HSD100PXN1) on it. They use the Galaxy Touch device .And the touch screen is included with the LVDS1 display. Hope this can help you.
Have a great day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------