I referred to the following manual.
i.MX 6Solo/6DualLite Applications Processor Reference Manual Rev.1, 04/2013
- Table 9-8. VPU decoding/encoding capabilities(P.479)
- Table 69-1. Supported Decoding/Encoding Standards(P.5681)
About the profile indicated here,
Do these have any HW Limitation?
For example,
Can VPU of i.MX6Solo decode any files encoded by H.264_BP?
Best Regards,
Yuuki
HI yuuki
Table 69-1. Supported Decoding/Encoding Standards
shows supported formats without HW limitations, only limitation
may be fps, usually it is 30fps in software BSPs (depends on board configuration
and porcessor loading). Also I would suggest to check below presentations for more
deep learning (one can ask local FAE for access)
FTF-CON-F0165Video and Image Codec and Data Pipeline for the i.MX 6 Series
FTF-CON-F0223Simplify Graphical User Interface and Video Integration for i.MX 6 Series Processors
http://www.freescale.com/files/abstract/overview/DWFREESCALE_OLL_ABS.html
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor-san,
In addition,
Would you teach the following contents?
1, Does VPU support all the motion compensation block sizes?
2, Does VPU support a multi-reference?
3, Does VPU support all nine Intra Prediction?
Best Regards,
Yuuki Murasato