About Lens calibration for surround view sample application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Lens calibration for surround view sample application

2,213件の閲覧回数
hsaito
Contributor I

We are using the camera is corrected only in the y-axis.

We wants to surround view application using this camera.

The attached image is a reference image of the camera's video output.

Does OcamCalib support this camera calibration?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,908件の閲覧回数
Kuniyan
Contributor I

Hello, I would like to know how to use OCamCalib toolbox for Matlab.
Is OCamCalib toolbox able to correct the camera which Y-axis(Red line) has already been corrected as shown in Fig. 1?
If OCamCalib toolbox able to correct the camera like above, please tell me how to use OCamCalib toolbox in order to complete the Goal image(Fig.2) in Surround view application finally. Please refer to attached. Please suggest any possible solution for this problem as soon as possible.

0 件の賞賛
返信

1,865件の閲覧回数
Kuniyan
Contributor I

Hello, I would like to know how to use OCamCalib toolbox for Matlab. The attached photos are 10 images of the checkerboard taken with 190 degree fisheye camera. Is it possible to correct the lens from these images using OcamCalib toolbox? However, this fisheye camera has already been corrected in the Y-axis direction by the camera itself.

0 件の賞賛
返信

1,864件の閲覧回数
Kuniyan
Contributor I

I have attached the remaining 5 images.

0 件の賞賛
返信

2,157件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There are two documents show the details. Please read :

Surround View Application User's Guide

Surround View Application Reference Manual

0 件の賞賛
返信

2,056件の閲覧回数
Kuniyan
Contributor I

Hello, I would like to know how to use OCamCalib toolbox for Matlab. 
If I use OCamCalib for a camera whose Y-axis has already been corrected on the camera itself (Fig. 1), Fisheye distortion will become stronger as shown in Fig. 2. Please tell me how to successfully remove Fisheye distortion from X-axis only.  Please refer to attached.

0 件の賞賛
返信