About LVDS output resolution of i.MX 6Quad.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About LVDS output resolution of i.MX 6Quad.

ソリューションへジャンプ
2,374件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Is i.MX6Q possible to output the timing of "800(H)x1280(V)" via LVDS?

Refer to attached detail file.

(i.e. I'd like to know the maximum size with horizontal line.)

Best Regards,

Keita

ラベル(6)
0 件の賞賛
返信
1 解決策
2,218件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible, LDB has limitation only on perfomance IMX6DQRM

39.4.1 Input Parallel Display Ports:

For single input data interface case: Up to 170 MHz pixel clock (WUXGA

1920x1200)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,219件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible, LDB has limitation only on perfomance IMX6DQRM

39.4.1 Input Parallel Display Ports:

For single input data interface case: Up to 170 MHz pixel clock (WUXGA

1920x1200)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,218件の閲覧回数
keitanagashima
Senior Contributor I

Dear Igor,

Hello.

Thank you for your reply.

>For single input data interface case: Up to 170 MHz pixel clock (WUXGA 1920x1200)

I think that i.MX6 support up to 170 MHz (up to UXGA) in Dual Channel.

Refer to attached file again.

We'd like to use the resolution of 800(H) x 1280(V).

Is it possible to use the display of 1280 vertical lines.

[This is over the 1920(H) x 1200(V)]

Best Regards,

Keita

0 件の賞賛
返信
2,218件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes possible.

Best regards

igor

0 件の賞賛
返信