About LPCM playback by Gstreamer with i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LPCM playback by Gstreamer with i.MX6DL

645 Views
yuuki
Senior Contributor II

Dear all,

We run Yocto Linux BSP on i.MX6DL-SABRE-SD board.
- Linux BSP: L3.10.53

We want to run LPCM (MPEG TS) playback by using Gstreamer.
- Gstreamer version 1.2.3.

However, though the error does not occur, we cannot playback.


Does Gstreamer of L3.10.53 BSP support LPCM playback of MPEG TS?


When LPCM playback is not supported,
Would you add this function to plugin?

May I have advice?

Best Regards,
Yuuki

Labels (3)
Tags (1)
0 Kudos
Reply
3 Replies

511 Views
yuuki
Senior Contributor II

Dear all,

It is the item which is important in our system.
May I have a response?

Best Regards,
Yuuki

0 Kudos
Reply

511 Views
joanxie
NXP TechSupport
NXP TechSupport

did you try gplay? if failed, pls send the ts file to test.

0 Kudos
Reply

511 Views
yuuki
Senior Contributor II

Dear Joan Xie-san,

Thank you for your support.

I prepared for Ts file.
However, this file includes contents for our internal inspection.
Therefore, we cannot upload it to this thread.

Please tell me the method to send this file only to you.

We suspect that Auirdemux may not support the gstreamer1(decoder-audio/x-private2-lpcm)()(64bit).

We think that aplay has the same problem if Auirdemux does not support gstreamer1(decoder-audio/x-private2-lpcm)()(64bit).

Would you confirm it about the following question?

<Question>
- Does Auirdemux of Gstreamer version 1.2.3 support gstreamer1(decoder-audio/x-private2-lpcm)()(64bit)?

- Does the decoder plug in to support gstreamer1(decoder-audio/x-private2-lpcm)()(64bit) exist?


If these answers are No

- Is there the method to add gstreamer1(decoder-audio/x-private2-lpcm)()(64bit) to Auirdemux of Gstreamer version 1.2.3?

Best Regards,
Yuuki

0 Kudos
Reply