About LDO_SoC supply in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LDO_SoC supply in i.MX6DQ.

Jump to solution
846 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. Refer to "50.2 Digital LDO Regulators" in IM6DQRM(Rev.2).

There is below description.

"The SOC regulator powers the rest of the digital logic on the chip."

What is the "rest of the digital logic"?

And, what case increases current consumption in the logic?

Best Regards,

Keita

Labels (5)
0 Kudos
Reply
1 Solution
753 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

SoC is other digial circuitry not depicted on Figure 50-1,

for example CCM. Its current consumption increases when,

for example, PLL frequency is increased.

Best regards

igor

View solution in original post

0 Kudos
Reply
3 Replies
753 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

SOC regulator powers powers HDMI_VP, SATA_VP, PCIE_VP

depicted on Figure 50-1.

>what case increases current consumption in the logic?

Current consumption in the logic is increased when logic

works on higher frequencies and temperatures, at low frequency

current is less, when some module clocks are gated with

CCM_CCGRn registers, then its current has lowest current consumption.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
753 Views
keitanagashima
Senior Contributor I

Dear Igor,

Hello. Thank you for your reply.

> SOC regulator powers powers HDMI_VP, SATA_VP, PCIE_VP

OK. Thank you.

Refer to below block.

What is "SoC" block? And, what case increases current consumption?

i.MX6Q_PMU.PNG

Best Regards,

Keita

0 Kudos
Reply
754 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

SoC is other digial circuitry not depicted on Figure 50-1,

for example CCM. Its current consumption increases when,

for example, PLL frequency is increased.

Best regards

igor

0 Kudos
Reply