Dear All,
Hello. Refer to "50.2 Digital LDO Regulators" in IM6DQRM(Rev.2).
There is below description.
"The SOC regulator powers the rest of the digital logic on the chip."
What is the "rest of the digital logic"?
And, what case increases current consumption in the logic?
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita
SoC is other digial circuitry not depicted on Figure 50-1,
for example CCM. Its current consumption increases when,
for example, PLL frequency is increased.
Best regards
igor
Hi Keita
SOC regulator powers powers HDMI_VP, SATA_VP, PCIE_VP
depicted on Figure 50-1.
>what case increases current consumption in the logic?
Current consumption in the logic is increased when logic
works on higher frequencies and temperatures, at low frequency
current is less, when some module clocks are gated with
CCM_CCGRn registers, then its current has lowest current consumption.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
Hello. Thank you for your reply.
> SOC regulator powers powers HDMI_VP, SATA_VP, PCIE_VP
OK. Thank you.
Refer to below block.
What is "SoC" block? And, what case increases current consumption?
Best Regards,
Keita
Hi Keita
SoC is other digial circuitry not depicted on Figure 50-1,
for example CCM. Its current consumption increases when,
for example, PLL frequency is increased.
Best regards
igor