About LCD IF max resolution of i.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About LCD IF max resolution of i.MX6UL

ソリューションへジャンプ
1,788件の閲覧回数
yuuki
Senior Contributor II

Dear all,

The parallel display port of i.MX6UL supports resolution of maximum WXGA (1366 x 768).

We need resolution of 1280 x 800.

Can display port support resolution of 1280 x 800?

Best Regards,

Yuuki

ラベル(1)
0 件の賞賛
返信
1 解決策
1,542件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes it can support, probably with slower fps, as there are

no hardware limitations limited only to WXGA.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,543件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

yes it can support, probably with slower fps, as there are

no hardware limitations limited only to WXGA.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,542件の閲覧回数
shanashiro
Contributor I

Dear all,

How to calculte fps when resolution of 1280 x 800 ?

Best Regards,
Seiso

0 件の賞賛
返信