Dear all,
We want to make application of JPEG Decode using VPU.
We have the following questions.
May I have advice?
[1]
Files of different size and format cannot be decoded in succession.
When some JPEG files of the different size are decoded in succession,
Is there the method to decode in succession without performing Open/Close of VPU_Decoder?
If it is possible, may I have advice about a setting method?
[2]
A "JPEG decode result" changes by file format(before decoding).
(JPEG file => decode => YUV420 or YUV444 format)
Is there the method to fix the format of the decoded file?
(For example, formats are only YUV444.)
If it is possible, would you tell me the method with a format as RGB?
[3]
After Jpeg decode, would you tell me the method to resize?
May I have advice?
Best Regards,
Yuuki
已解决! 转到解答。
Hello,
In order to use hardware accelerated (via VPU) codecs under Android, Freescale
is offering additional package (Extended Multimedia Feature Package) to extend
Android KK4.4 and Android L5.0 core functionality. These packages will not be
generally available on Freescale.com and is not supported in Community.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
In order to use hardware accelerated (via VPU) codecs under Android, Freescale
is offering additional package (Extended Multimedia Feature Package) to extend
Android KK4.4 and Android L5.0 core functionality. These packages will not be
generally available on Freescale.com and is not supported in Community.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------