About Internal LDO output accuracy in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About Internal LDO output accuracy in i.MX6DQ.

1,189 次查看
keitanagashima
Senior Contributor I

Dear All,

Could you tell me the output accuracy of Internal LDOs  in i.MX6DQ? (+- x%?)

PS,

Internal LDOs can set the 25mV step.

So, I think that てthe spec is within +- 25mV.

Best Rgards,

Keita

标签 (3)
0 项奖励
回复
2 回复数

1,017 次查看
Yongxin
NXP Employee
NXP Employee

Hi Keita,

The outputs of the internal LDOs are likely to be in the range of +/-2% in i.MX6DQ.

Best Regards,

Yongxin

0 项奖励
回复

1,017 次查看
keitanagashima
Senior Contributor I

Dear Yongxin,

Hello. Thank you for your reply.

But, If your answer was right,

For example,

VDDPU LDO outputs (VDD_SOC_CAP and VDD_PU_CAP) must less than 1.3 V.

If one set VDDPU LDO outputs = 1.275V, output accuracy was +/-0.0255V (+/-25.5mV).

The output voltage looks spec-out with VDDPU LDO outputs = 1.275V.

Really?

Best Regards,

Keita

0 项奖励
回复