About Internal LDO output accuracy in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Internal LDO output accuracy in i.MX6DQ.

1,193 Views
keitanagashima
Senior Contributor I

Dear All,

Could you tell me the output accuracy of Internal LDOs  in i.MX6DQ? (+- x%?)

PS,

Internal LDOs can set the 25mV step.

So, I think that てthe spec is within +- 25mV.

Best Rgards,

Keita

Labels (3)
0 Kudos
Reply
2 Replies

1,021 Views
Yongxin
NXP Employee
NXP Employee

Hi Keita,

The outputs of the internal LDOs are likely to be in the range of +/-2% in i.MX6DQ.

Best Regards,

Yongxin

0 Kudos
Reply

1,021 Views
keitanagashima
Senior Contributor I

Dear Yongxin,

Hello. Thank you for your reply.

But, If your answer was right,

For example,

VDDPU LDO outputs (VDD_SOC_CAP and VDD_PU_CAP) must less than 1.3 V.

If one set VDDPU LDO outputs = 1.275V, output accuracy was +/-0.0255V (+/-25.5mV).

The output voltage looks spec-out with VDDPU LDO outputs = 1.275V.

Really?

Best Regards,

Keita

0 Kudos
Reply